cancel
Showing results for 
Search instead for 
Did you mean: 

STBC15 wiring of open drain output pins

EC.3
Associate III
Hello,
 
I see there are two open drain output pins on the STBC15: CHGINOK and PG. If I don’t need to read the CHGINOK and PG status, can they either be left floating or connected to ground, without needing to add an external pullup?
 
Please confirm if this is the correct understanding.
 
Thanks
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

The CHGINOK and PG pins are open drain outputs. If you do not want to query them, you can either let them float or connect them to GND to be on the safe side.

Hope that helps?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

The CHGINOK and PG pins are open drain outputs. If you do not want to query them, you can either let them float or connect them to GND to be on the safe side.

Hope that helps?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.