2021-11-09 04:28 AM
I can see that the datasheets and app notes say that the PWM input can operate at up to 20kHz PWM frequency, but I can't see anywhere anything that discusses using a PWM signal on the INA and INB inputs. Can we apply a 20kHz PWM signal to these inputs, or do they have a much lower operating frequency as they are intended for direction control only?
2021-11-15 02:40 AM
Hello ST folks - can anyone please help with this?
2021-11-16 04:01 AM
Don't worry - I've now answered this question, around 3kHz.