cancel
Showing results for 
Search instead for 
Did you mean: 

We have to design programmable power supply as per below spec 1. Vin: 230VAC, 50Hz 2. Vout: 0-120VDC or 20-120VDC, 12A max (variable with external control voltage from 0 to 5V) 3. Temp: -20 to +55 C Please suggest us any part number.

SA.9
Associate

Hi,

We have to design programmable power supply as per below spec

1. Vin: 230VAC, 50Hz

2. Vout: 0-120VDC or 20-120VDC, 12A max (variable with external control voltage from 0 to 5V)

3. Temp: -20 to +55 C

Please suggest us any part number, this is for Ground based application. Is SG2525 is suitable? If so please suggest any reference design

0 REPLIES 0