2017-08-16 05:40 AM
We have purchased an EVLpowerstep01 and a STEVALPCC009V2. We installed the SPINFamily software on our Windows10 64-bit computer and on connection it states 'The FW version is not the last, upgrade to 2.7'. The doco states this is done via the IBUUI updater, but when this runs it states it cannot access the IBUUI.inf driver. However, it is looking in the wrong folder (an XP folder) and apparently cannot see the IBUUI.inf file sitting there. This is a poor start to our initial research into using the powerstep01 in our new high power stepper controller. What are our next steps?
Ron Kreymborg
R&D ManagerKremford Pty Ltdkremford.com.auSolved! Go to Solution.
2017-08-24 06:21 AM
Hello Ron,
unfortunately the IBUUI Updater is based on old drivers and they are probably not supported by Windows 10.
I suggest you to update the firmware of the STEVAL-PCC009V2 through SWD as described in Appendix A of the software's UM (
)2017-08-16 05:58 AM
This is primarily a user forum, consider registering your project with a local sales/support office, and discussing with an FAE
2017-08-16 06:42 AM
I am a user with a user question. Are you saying there are no ST people paying attention to this forum?
2017-08-16 09:34 AM
I'm saying it is a user-to-user forum, engineering support is done through traditional business channels, not via social media.
2017-08-24 06:21 AM
Hello Ron,
unfortunately the IBUUI Updater is based on old drivers and they are probably not supported by Windows 10.
I suggest you to update the firmware of the STEVAL-PCC009V2 through SWD as described in Appendix A of the software's UM (
)2017-08-24 08:14 AM
Thanks Enrico, that was the problem. I purchased an ST-LINK/V2 and updated the firmware in the STEVALPCC009V2. The SPIN Software now drives the Powerstep01 as it should. Regards, Ron.
2019-07-11 04:55 AM
Great job, ST!
Plan for success:
Now, seriously, you guys should fire your crack dealer!
2019-07-11 05:29 AM
I have achieved success programming the gizmo: