cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L7CX et VL53L8CX

Freedy
Associate II

I recently purchased a VL53L7CX and VL53L8CX, so I wanted to test the Motion Indicator functionality for each zone to show if the targets moved and how they moved via SPD of the software by STM except that there, when two people present themselves in front of the sensor, we only see one person
How to do it?

1 ACCEPTED SOLUTION

Accepted Solutions
OlivierL
ST Employee

I confirm that SPD is able to detect and monitor the X/Y/Z position of up to 4 different persons, provided those persons are far enough from each others to be identified/separated within the 8x8 depth map...

View solution in original post

6 REPLIES 6
John E KVAM
ST Employee

SPD will track the first person into the FoV. This is because we were trying to sell it into the PC market and we assumed we were following the main user. And when 'he' left we assumed we could shut down the PC. We really did not build in a second user. 

But here is how you do it...

Run through all the zones looking for those zones that have more-or-less the same distance. That 'clump' of zones is probably one of your users. Now find the center of mass of that clump. Then look for another clump. That's your second user. 

The trick comes when you have to decide if it's a user or a chair. One can assume chairs don't move. But sometimes they do. And if they are tall chairs, they even have the right shape - more or less. 

Handle the corner cases and you are all set.

 -john


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.


Except that in the presentation video of VL53L7CX and VL53L8CX you illustrated multitarget detection which led me to buy it for a project even though this is not the case
Communicate what is real!

OlivierL
ST Employee

I confirm that SPD is able to detect and monitor the X/Y/Z position of up to 4 different persons, provided those persons are far enough from each others to be identified/separated within the 8x8 depth map...

Let me complete my reply with more details...

To visualize the (X, Y, Z) position of each person in front of the sensor, you can use the SPD EVK GUI and use the Users Analysis widget as shown below...

OlivierL_0-1741296698461.png

If you prefer using your favorite Serial Com emulator like TeraTerm, you'll get this kind of outputs showing the same kind of information...

OlivierL_1-1741296769657.png

From a pure programmatic point of view, below is a pseudo-code giving the name of the fields of interest to get access to the Multi-Human outputs...

 

 

// Users outputs (including intruders)
SPD_Data.USR_Data.nb_of_users
SPD_Data.USR_Data.intruder_alert
for (i=0;i<4;i++){
  SPD_Data.USR_Data.user_properties[i].obj_prop.CoM_pos.x
  SPD_Data.USR_Data.user_properties[i].obj_prop.CoM_pos.y
  SPD_Data.USR_Data.user_properties[i].obj_prop.CoM_pos.z
  SPD_Data.USR_Data.user_properties[i].intruder
}

 

 

More details can be found in the SPD EVK GUI User Manual...

Hope this helps...

Freedy
Associate II

Translating to English
I need assistance to run the SPD project under STM32CUBE IDE please
The code starts and determines the type of sensor and at the time of initialization the program crashes

John E KVAM
ST Employee

This site works better if each issue is under a new post. Having a conversation makes it hard for people to follow and track. 

-----

That's not much help. But during the init stage, the MCU needs to download some 80K of firmware to the sensor. This is where most people have trouble. 

If you are NOT using an STM32 (And we think you should - but we are clearly biased) then there is an issue of byteswap, as well as possible limits on the length of the I2C or SPI transfer. 

---

Try this... Open a new topic. Describe what you can. And provide where your program is failing. Then we can find a solution.

- john


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.