2025-01-01 9:26 PM
Hi,
Can you please tell me the function of status pin? Is this pin can be used as feedback pin and connect to mcu?
If not used, what to do? In datasheet, table 2 is given for unused and not connected pins, but it is not clearly.
2025-01-02 1:40 AM
Table 2 of the data sheet only uses the letter X to show how the pins may be connected. For pin STATUS, this means that it may float, but may not be permanently connected to GND.
For the function of the STATUS pin, it is best to take a look at table 6 and the waveforms in fig 6.
Hope that helps?
Regards
/Peter