cancel
Showing results for 
Search instead for 
Did you mean: 

Use of an NTC temperature feedback device (non-semiconductor junction)

luke23
Associate III
Posted on March 24, 2014 at 02:53

Hi

The MC Toolbox wizard (and presumeably the MC library itself) seems to support only the use of p-n junction temperature feedback devices (25mV/degC), with support to alter coefficients.

In our application we are using an NTC thermistor.  Any plans to support these additional devices, please?  Simple parametric would be required to specify the temperature transfer function to the library.

Thanks

Luke

#ntc-temperature-diode
1 REPLY 1
Gigi
ST Employee
Posted on March 31, 2014 at 09:48

Yes, we plan to extend the support also for negative slope and maybe for other kind of transfer functions.

Ciao

Gigi