2021-12-30 03:12 AM
2022-01-24 08:26 AM
Yes, I use the TACHO pin from J8 and it is correctly synchronized with H1 signal. Besides, I have added a 0.1 uF capacitor parrallel to the '10 nF' and I got 2.88 ms at the TACHO pin. With this result, I believe the capacitor C11 on the Eval6235Q R1.1 wasn't 10 nF, but only 2 - 4nF.