cancel
Showing results for 
Search instead for 
Did you mean: 

Has any information on the PPAK SMD PCB land pattern . Im trying to use a LF50AB regulator and I cant find a PCB land pattern drawing anywhere , searched STM etc Thanks Dave

dave239955
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @dave239955​, to the community!

Footprints are typically included in newer datasheets, but unfortunately this is still missing here. In the meantime, ST has a cooperation with UltraLibrarian, which is also referred to via the CAD Resources tab, but unfortunately the footprint for the PPAK 5L in connection with the LF50ABPT-TR is still missing, too.

Workaround: the LDFMPT-TR also uses an absolutely identical package, so you can use its footprint even if it is a different LDO. Simply select tab CAD Resources and get the footprint from there.

Is that helpful?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
Peter BENSCH
ST Employee

Welcome, @dave239955​, to the community!

Footprints are typically included in newer datasheets, but unfortunately this is still missing here. In the meantime, ST has a cooperation with UltraLibrarian, which is also referred to via the CAD Resources tab, but unfortunately the footprint for the PPAK 5L in connection with the LF50ABPT-TR is still missing, too.

Workaround: the LDFMPT-TR also uses an absolutely identical package, so you can use its footprint even if it is a different LDO. Simply select tab CAD Resources and get the footprint from there.

Is that helpful?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Paul1
Lead

You can get footprints at

  • SnapEDA.com
  • mouser.ca (See ECAD icon on page for part, I see a few different LF50AB)

Paul

dave239955
Associate II

Thatnk you paul sadly PPPAK is not available from Mouser, or SnapEDA, the DPAK D2PAK versions are

thanks Peter that did the trick

Paul1
Lead

--deleted--

Please don't use the footprint from the document on bdtic.com as it is from 2004 and much older than the current one mentioned above.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.