2024-08-20 12:14 AM
Hi All,
I have developed my own Evalboard for the STWBC2-HP based on the STEVAL-WBC2TX50. Now i have flashed the stdes-50w2cwbc_FW_v1.0.0.0.hex firmware to the board and the Software shows the following. The power transfer does not work. Do you have any suggestions why that is so?
Thank You
2024-08-20 12:32 AM
2024-08-20 12:40 AM - edited 2024-08-20 12:51 AM
Ok thank you.
But with this hex file loaded, it is nearly impossible to connect to the IC via UART. The most time this error occurs when connecting:
Is it possible to initate the Calibration via SWD interface with the STM32 Cubeprogrammer?
After a few times trying to connect it worked, but now i get the following message: SCHEDULER-MSG-ERROR
The error log is attached.
2024-08-20 12:55 AM
Hi
Please erase all and download again, i have retest and do not have connect issues.
2024-08-20 01:31 AM
I have erasedthe memory and downloaded it again.
But the problem still occurs. It seems that there is another problem on my board.