2023-08-16 12:57 PM - last edited on 2023-08-16 11:32 PM by Peter BENSCH
Hello,
I am using the STUSB4710AQ1TR to charge some USB-C devices at the default 45W. I am operating in a mode that's only charging (no data communication). To do this, I used the recommended application schematic provided in the datasheet. My input voltage (Vin) is a 24V source created by a TI LM5116 (because my input voltage for our system is 48V and the ST1S14PHR cannot handle that high).
When I am under load, the circuit works as intended and achieves the 45W power charging. However, when there is no load, I hear this clicking noise and the output of the LM5116 is much more variable. I've included an oscilloscope shot of the input voltage at no load.
I am using the same LM5116 circuitry to power some USB-A circuitry at 5V, and it does not experience this oscillation.
Does anyone know what would cause this?
2023-08-16 01:22 PM
2023-08-17 07:27 AM
Hello,
Thank you for the reply. I was only mentioning the LM5116 so it was known that the power supply was from a switching source. I'm using the same one on the USB-A and this does not occur, even if there's no load. So I am trying to find the difference and the USB-C charging portion, which is completely an ST product, is the only difference. So wouldn't it make sense to start there?
2023-08-17 11:52 AM
when there is no load, I hear this clicking noise and the output of the LM5116 is much more variable
Computer ATX power supplies usually have a load resistor.
2023-08-17 12:44 PM
Interesting.
So they constantly have something to draw a little bit of current just to satisfy the needs of the converter? I was not aware of that! (Still green to the field haha).
Thank you for this!!