cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-PTOOL1V1 Who has the sample code for STEVAL-PTOOL1V1? I can't find it on ST.com. thanks a lot.

Dylan.Dong
Associate II
 
3 REPLIES 3
Cristiana SCARAMEL
ST Employee

Hello @Dylan.Dong​ and welcome to the ST Community.

As you can read in the board documentation (data brief and user manuals), you can find a firmware example in the STM32 Motor Control SDK (X-CUBE-MCSDK-Y).

The firmware example included in the STM32 MC uses position feedback from Hall effect sensors, with debugging and programming capability available through the SWD interface and the direct firmware update feature.

Let me know if this info is useful to you, if yes please "Select as Best" label to close the topic.

If you feel a post has answered your question, please click "Accept as Solution"

Sorry I​ did not find the firmware example in X-CUBE-MCSDK-Y. Can you help me find it? Thanks.0693W00000HqEeHQAV.png

Hi @Dylan.Dong​ which SW version have you installed?

The STEVAL-PTOOL1V1 is supported by Rev Y 5.5.2 and following.

If you feel a post has answered your question, please click "Accept as Solution"