2017-04-04 8:25 AM
/********* This question is also asked at ''Power Management and Motor Control > Discussions''
*********/
Hi,
I am trying to use the STEVAL-PCC009V2 & EVAL6470H boards using the SPIN
Family Evaluation Tool (Version 3.2)
However when I try to connect to the board I get the following error:
I have managed to locate the below hex file at the following location:
C:\Program Files (x86)\STMicroelectronics\SPINFamily Evaluation Tool 3.2\Firmware
I have tried to download the hex file below onto the board using Keil uVision but I am getting the following error in the Build Output.
It should be noted that I was able get older versions of the SPINFamily Evaluation Tool to work.
If anyone has any solutions to this problem or has a link to Version 3 of the Evaluation Tool I would greatly appreciate it.
Kind Regards,
Ernest Cooke
#powerstep01 #dspin-gui #pcc009v2-eval6470h-spinfamily #keil-uvision