2017-04-04 08:31 AM
Hi,
I am trying to use the STEVAL-PCC009V2 & EVAL6470H boards using the SPIN
Family Evaluation Tool (Version 3.2)
However when I try to connect to the board I get the following error:
I have managed to locate the below hex file at the following location:
C:\Program Files (x86)\STMicroelectronics\SPINFamily Evaluation Tool 3.2\Firmware
I have tried to download the hex file below onto the board using Keil uVision but I am getting the following error in the Build Output.
It should be noted that I was able get older versions of the SPINFamily Evaluation Tool to work.
If anyone has any solutions to this problem or has a link to Version 3 of the Evaluation Tool I would greatly appreciate it.
Kind Regards,
Ernest Cooke
#dspin #pcc009v2-eval6470h-spinfamily #dspin-gui #powerstep01 #keil-uvision2019-04-24 01:49 PM
BUG at SPINFamily Evaluation Tool (STSW-SPIN002)
There is a bug when I use ihm03a1 with SPINFamily Evaluation Tool. I am creating new settings for my motor, select Voltage mode, and resistance > 2 Ohm. So SPINFamily Evaluation Tool throw fatal exception.
2019-05-12 07:13 PM
My motor has 5 Ohms resistance. When I try to set 5 Ohms at SPINFamily tool for ihm03a1 - application crash! Is it a bug of application?
2021-01-06 10:28 AM
2023-11-20 09:35 PM
Thanks for your instruction. It works for me !