cancel
Showing results for 
Search instead for 
Did you mean: 

SpinFamily crashes after connection on WinXP SP3

crenner_twi
Associate
Posted on February 03, 2014 at 06:10

Hello,

  I am seeing a error with the ''SPINFamily Evaluation Software'' when running on Windows XP sp3 on three different platforms.

I was able to get the software to operate on a Windows 7 platform, so I am reasonably confident that I am starting up everything correctly and that my hardware is okay.

I see a crash as soon as I connect to the board.

Details:

Windows XP sp3 system [Windows NT 5.1 Build: 2600]

.Net 4.0 [fresh .NET 4.0 install, fresh sp3 install]

SPINFamily Evaluation Software (L6480 selected) [fresh install]

According to the message at the bottom of the Spin window the board did connect:

Board connected (BR_4MHz) FW Version 0.0

This matches what I saw on a windows 7 system that I used to validate that my hardware was okay.

Looking a little closer at the error report:

EventType : clr20r3     P1 : gui.exe     P2 : 1.2.5071.18356     P3 : 528b2b58

P4 : mscorlib     P5 : 2.0.0.0     P6 : 471ebc5b     P7 : 1295     P8 : 14     

P9 : system.missingmethodexception     

Is there a way around this error?

Thank you,

- Charles.

#cspin
1 REPLY 1
Gigi
ST Employee
Posted on March 11, 2014 at 09:34

Ciao Charles

I suggest to post this question in the

https://my.st.com/public/STe2ecommunities/motordriver_ics/Lists/Motor%20Driver%20ICs%20and%20Boards/AllItems.aspx

forum.

Thanks

Ciao

Gigi