2014-01-27 10:00 PM
Hi,
I have an SPEVAL-PCC009V2 with EVAL-6470H setup controlling one stepper motor very effectively. I want to control two motors but would prefer to do this using separate chip selects for each L6470 instead of using the daisy chain configuration described in AN3991. Is is possible to do this? Possibly related to the above question, is is possible to extend the scripting language in dSPIN to include control of additional IO ports in the STEVAL-PCC009V2? Thanks, Bob2014-03-11 1:33 AM
Ciao Robert
I suggest to post this question in the forum. Thanks Ciao Gigi