2014-10-21 6:30 AM
hello,
I have a EVAL6480H board and try to connect it with a Atmel Xmega. But on the SDO line is always the Byte which I send before on SDI. Does I Need to make some initalisation before start a communication? I choose SPI Mode 3 and a frequency of 250kHz. Hope someone can give me advise. #l6480 #l6482-spi #spi-config-problem2016-01-23 8:01 PM
Hi,
Is it solved? I have meet the same issue with the boardEVAL6482H, my MCU is the dsPIC30F5011, i
also checked all the SPI signals, they are all flowing the spec. anyone can help ?