cancel
Showing results for 
Search instead for 
Did you mean: 

Replace L6569 in an electronic ballast with L6571

pleite
Associate

Hello,

Can I directly replace L6569 with L6571 High Voltage Half Bridge Driver with oscillator?
I've notice that in L6571 doesn't have the internal bootstrap driver.

Thanks.

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @pleite, to the community!

The L6569 was discontinued years ago. However, you should be able to replace the L6569 with the L6571 if you connect the external bootstrap diode (fast recovery one) between Vs and BOOT, which the L6569 does not need because of the internal synchronous bootstrap driver.

Please note, however, that the dead time of the L6571B is 0.72µs, whereas the L6569 had a dead time of 1.25µs.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.