2023-04-24 9:55 PM
Hello!
I would like to get information on the wireless charger receiver Part no: STWLC38.
I am looking for a wireless power receiver that supports:
10.5V-11V voltage output
0.65A current output
STWLC38 - per the datasheet it appears to support the above requirement. I would like to confirm on the same.
Max power 15W receiver side; Vout_max - upto 20V; Vout can be set Firmware configurable VOUT_SET; Vout output current - 2A (rms)
Can you suggest the recommended evaluation kit and transmitter for the receiver to achieve the above requirement.
Currently, I do not see a stock available for the eval kit. Is there a sales contact to check for availability and lead time on samples?
Let me know your input!
Regards and Thanks
Madhu
2024-01-08 12:36 AM
Dear Customer
For support of 10.5-11V Vout voltage, it is recommended
to use EPP transmitter and set the EPP Vout Set to 10.5V.
Maximum power 5W is only BPP Transmitter, 15W is EPP Transmitter.
For high power we recommended to use other STWLC product
https://www.st.com/content/st_com/en/search.html#q=STWLC-t=products-page=1