cancel
Showing results for 
Search instead for 
Did you mean: 

DTS on the STWLC38

baymax
Associate

What is DTS used for?

And can I configure the following set of registers on through I2C to send and receive data in-between 2 STWLC38s through the main coil ? 

Does this Qi IC have a detailed user maual?

baymax_0-1699517265439.png

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
willzhou
ST Employee

DTS is the feature of Qi standard what allows
the communication between receiver and transmitter. The STWLC38 is RX only for Mass Market.

If you want TX to transfer DTS, please use STWBC2, ref to https://www.st.com/en/power-management/stwbc2-hp.html

 

Also there is example code here

https://github.com/STwirelesscharger/Python_FT260_ST_WLC/blob/main/a5_wlc38_send_recv_dts_packet.py

 

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
willzhou
ST Employee

DTS is the feature of Qi standard what allows
the communication between receiver and transmitter. The STWLC38 is RX only for Mass Market.

If you want TX to transfer DTS, please use STWBC2, ref to https://www.st.com/en/power-management/stwbc2-hp.html

 

Also there is example code here

https://github.com/STwirelesscharger/Python_FT260_ST_WLC/blob/main/a5_wlc38_send_recv_dts_packet.py

 

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.