‎2019-04-14 4:50 AM
Hi,
We have built devices that run on batteries and serve a specific task. For the future we also want to offer a wired solution, for better user experience and more features, that would drain the batteries faster. Since the wired solution already requieres hardware wiring, a remote readout of statistics of each node device, would be a very nice option.
A 4-wire solution (2 PWR / 2 Bus) would result in complex installation because alot of clamp terminals or even specific cable (twist pair) would be needed. A 2-wire (power) solution would offer ease of installation, because the power wires just can be connected with "cut-in" connectors
The physical layout of a node group (master with nodes) would be the following:
I spotted a few powerline modems from ST, but im unsure which of the devices would work fo our application.
Can someone recommend a device?
‎2019-04-14 6:40 AM
If you want to go with ST then try the ST7540 first. However I've always used the Maxim or Broadcom devices. Microchip, Cypress and many others also have them - and all mostly incompatible with one another of course =)
Or for an even simpler solution given your low speeds connect the USART to a one-wire mode line transceiver IC and connect it to a home-brewed inductor/capacitor splitter on the positive power rail.