2013-08-08 11:17 AM
I want to control a stepper motor (
http://pt.farnell.com/astrosyn/163/stepper-motor-1-8deg-5v/dp/9598650
) with L9942 from ST.But i have some problem because the motor dont rotate uniformly (lose some step):2014-02-02 10:41 AM
The STEP signal is an input signal and it should be generated by a microcontroller or by an external circuitry.
Checking the scope-snapshot, the duty cycle of the STEP signal is not constant. this behaviour can be the source of the problem you claimed.2014-07-09 12:22 PM
Good morning,
I would like to know how you manage to use the SPI protocol with the L9942 driver. I doesn't manage to use it so far...Thank you in advance,Thomas.2014-07-14 09:19 AM
dear Thomas,
The info you need are reported in the datasheet Please check chapter 5 and 6. Figure 10 and figure 11 are showing the timing diagrams. Best regards, Marco.