L9823 as Input?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-24 4:15 AM
I am using L9823 in my design to drive the outputs. I also want it to behave as input so that I can connect IO module. How can I use it as input?
Thanks in advance
- Labels:
-
Motor Control Hardware
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-05-15 5:13 AM
On top of what is reported in the DataSheet, what is not clear? Please, could you better specify what is unclear?
Thanks for your feedback
Best Regards
Luigi
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-05-15 10:22 PM
As L9823 is an output driver IC, I wanted to use it as input also. I need to connect IO devices in my design on same line. i.e. the user can change the module as per his requirement from Input to output or vice versa. As L9823 is an output driver IC, I don't want to use separate hardware for Input detection in case input module is connected. So I am thinking of using fault detection feature as input.
Is it a good design to use fault detection feature as input?
Thanks for the feedback.
Regards,
Sourabh