2013-09-30 8:34 PM
Hello,
I am using L6480 stepper motor driver. I have connected my board with SPIN software. If I run the motor status is shown as motor is operated. But in this case High side MOSFET's (HVGA1 & HVGB1) does not turn ON. There is no gate supply on this FET's. All other FET's are working. Kindly help me with the issue #l64802013-10-07 1:22 AM
The suggested configuration for the demonstration boards is the following:
VCC value = 15 V, UVLO threshold = 11 V (10 V on boot), Gate current = 64 mA, Controlled current time = 1 us, Dead time = 250 ns, Blanking time = 500 ns, Turn OFF boost = disabled. Regards EnricoHello,
I am using L6480 stepper motor driver. I have connected my board with SPIN software. If I run the motor status is shown as motor is operated. But in this case High side MOSFET's (HVGA1 & HVGB1) does not turn ON. There is no gate supply on this FET's. All other FET's are working. Kindly help me with the issue