2025-01-20 5:41 AM
I'm using a single L9963E and it works fine. However, I couldn't start daisy chain connection. When I consider BMS architectures in datasheet, all of them has L9963T transceiver to communicate with further IC. My custom PCB doesn't provide L9963T.
So I have two question:
1- Do I really need a transceiver for USE MULTİPLE l9963E slaves ?
2- Can I use the transceiver on EVAL-L9963E-MCU for this purpoeses?
Bear in mind, I'm using an external MCU, not built in SPC MCU chip.
Lastly, as I said, I can succesfully communicate single IC and I'm using a cable that has low capacitance.
2025-01-27 12:08 AM
Welcome @berg0vic, to the community!
Does it answer your questions?
Regards
/Peter
2025-01-27 1:52 AM
Hi,
Thanks for your response Peter. Now my current implementation has 4 wire SPI connection between MCU and L9963E. To use multiple IC I need to use transceiver between L9963E and MCU. Did I get right ? In this way, it will translate my signals to 2 wire isolated spi.
But according to datasheet the first node of chain can be one of these:
"The daisy chain and dual access ring topologies are based on a chain of BMS evaluation boards. The chain first node can be an AEK-POW-BMSWTX, an AEK-POW-BMSNOTX or an AEK-POW-BMSWTX. The remaining nodes must be all AEK-POW-BMS63EN evaluation boards."
As far as I understandalso "AEK-POW-BMSNOTX" does not contain L9963T and it can be use for the first chain of daisy chain. Thus my 4 wire SPI implementation can also be first chain of the daisy chain line. The datasheet is not very clear.
Best regards,