cancel
Showing results for 
Search instead for 
Did you mean: 

VIPER26K device fails when we tried to measure VDD pin voltage with respect to power ground

NSRPrasad
Visitor

We designed a buck converter with (300-800) input DC voltage and the output voltage is 24V.  The max load current is 150mA.  We noticed two issues here:

1. The device fails when we try to measure VDD pin voltage with reference to Power Ground (DC input ground).  Though the VDD voltage is with reference to device ground (pins 1,2,3,4,6), but why it should fail when we use power ground as a reference with a Digital Multimeter.  This has happened thrice and in all the cases, the device failed silently (no sounds, no physical damage etc.,).  All this happened at 150V DC input voltage itself.

2. In the second case, the device failed at 800V DC input when we tried to connect 100mA resistive load.  No probe is connected anywhere in the circuit.  However, we used the same compensation network as given in ST AN 5380 (15V, 1.5W buck converter and could not arrive at the values for 24V output voltage.  If the compensation network is a problem, can someone please help us in arriving at the correct values for compensation circuit.

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome @NSRPrasad, to the commnunity!

Please share your schematics you are testing.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
onistamodapk09
Visitor

Interesting issue you're encountering with the VDD pin and power ground reference. It could be related to floating grounds or potential difference between input and device ground causing unpredictable behavior. As for the compensation network , tweaking the values might require revisiting the design parameters specific to your output voltage and load current. Have you tried simulating the circuit with different compensation values before actual testing كاميرات مراقبة لمنزلك.