2022-08-17 6:58 AM
I don't need the motor control board, I have my own, I just need the power stage and the capacitor board.
2022-10-06 3:25 AM
Ciao
I', not a big expert of this board but I think it is possible to use it with a DC bus voltage of 12V.
Let's try. Maybe is just a documentation error.
Ciao
Gigi
2023-02-08 11:24 AM
Hello Sjenn,
I have to pilot a 12V motor with this board but I'm not sure if it's possible with this board,
Did you succeed to pilot it with 12V?
Thanks in advance,
2023-02-08 11:46 PM
Hi NBOUM.1
In the end we found a different solution so we never tested the board at 12V - sorry! However in my opinion - FWIW - it will work.
2023-02-08 11:52 PM
I will see if we can get the board up and runnign and test it at 12v.