cancel
Showing results for 
Search instead for 
Did you mean: 

The capacitors of STEVAL-CTM005V1 and the power side MOSFETS (STH315N10F7) are the components whose Will have 48V in their pins. can I have just 12V in their pin ?

NBOUM.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Cristiana SCARAMEL
ST Employee

Hello @NBOUM.1​ and welcome to the ST Community.

As you could read in this other thread, it should be possible to drive the board at 12V.

You just have to try.

If you feel a post has answered your question, please click "Accept as Solution"