2021-01-18 12:25 AM
2021-02-06 06:37 AM
I don't solve any issue, basic is is not a issue. the reason is that is ST's patent for catch current under one shunt architecture
ST will insert Zero vector (V0 or V7), in the special case for example when two of 3 phase duty cycle is to similar.
2021-01-19 05:37 AM
Hello @SkyWork,
Which boards are you using?
Control method?
Application ratings?
For a better support, please share any other useful info.
2021-01-22 02:03 AM
Hello @SkyWork,
do you still need Community support?
2021-01-26 04:54 PM
Hello @Cristiana SCARAMEL
I have clarified this issue thanks for your support
2021-02-04 07:02 AM
Hello @SkyWork,
could you share a summary about your issue and how you solve it.
In this way could help the Community members who might have similar concern.
2021-02-06 06:37 AM
I don't solve any issue, basic is is not a issue. the reason is that is ST's patent for catch current under one shunt architecture
ST will insert Zero vector (V0 or V7), in the special case for example when two of 3 phase duty cycle is to similar.