cancel
Showing results for 
Search instead for 
Did you mean: 

I am using STPM34 for measuring RMS voltages. When I measure grid voltages it's fine. But I read the inverter output voltage, the value is oscillating from 0 to 500v. Please help me to resolve this.

THANGAMUTHU
Associate II
 
6 REPLIES 6
Peter BENSCH
ST Employee
What is the inverter output voltage: AC or DC?
When AC: what frequency?
How did you connect the STPM34 to this voltage?
Regards
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
THANGAMUTHU
Associate II

Inverter Output voltage : 200 - 270V AC

Frequency : 50Hz

0693W000008xrHPQAY.jpg 

Javier1
Principal

we need to see te code aswell, did you probed the inverter output with an oscilloscope?

Maybe is much much noisier and spikey than you expect. (specially with no load attached)

Available for consulting/freelancing , hit me up in https://github.com/javiBajoCero
THANGAMUTHU
Associate II

V factor = VREF * (1 + (R1 / R2)) / (AU * CALIB_V * DPOW)

        = (1.18 * (1+ (810000/470))) / ( 2 * 0,875) = 116274,11

I factor = VREF / (AI * CALIB_I * DPOW * KSI * KINT )

        = 1.18 / (2 * 0,875 * 0,00260 * 1) = 25934,06

By using the above formula we calculated Voltage and Current. For Grid Voltage STPM34 is reading Correctly, we are facing the issue when reading inverter output AC voltage. I have attached waveforms across the VIP1 pin. I have changed the Capacitor across VIP1 pin 10nF to 100nF but also facing the issue same.0693W000008xtAVQAY.jpg0693W000008xtABQAY.jpg0693W000008xtA6QAI.jpg

that looks like a very noisy signal.....

What about triggering the ADC reading only when the pwm event?

Available for consulting/freelancing , hit me up in https://github.com/javiBajoCero
THANGAMUTHU
Associate II

Kindly Suggest proceeding further?

  1. Grid Input
  2. Inverter Input

0693W000008yTevQAE.png0693W000008yTelQAE.png