I am Finding wireless charging guru ▶ Heat comes out while Wireless charging.
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-07-10 9:18 PM
Hello everyone !
I am using STWBC86 and STWLC38 MCUs, using our own custom board.
The wireless charging was going well, but the problem is this.
[ When charging → put away the RX → put back the RX ] ...▶ the heat comes out from the RX MCU.
Any ideas to solve this issue ? Thank you.
Solved! Go to Solution.
Labels:
- Labels:
-
Discretes
10 REPLIES 10
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-01-23 9:22 PM
I started increase the load, from 100mA to 1,000mA in 100mA step. The Vout remains stable.
For our product, power could be 1.35 ~ 2.5W or so (300~500mA , by setting Vout 4.5 V - to 5.0 V).
I have to test further, but it seems the problem solved.
Thank You.

- « Previous
-
- 1
- 2
- Next »