2022-11-04 4:13 PM
Hi. I am interested in using the STEVAL-IPMM10B evaluation board to drive a BLDC motor with the voltage rating of 50 V. The evaluation board user manual says, it works for 125-400 VDC. Is there any way I can use this board for lower voltages? Thanks.
Solved! Go to Solution.
2022-11-06 11:16 PM
You're welcome!
Correct, you would have to adjust the voltage divider R1,2-R4 if you absolutely and against all expectations want to stay with the STEVAL-IPMM10B.
Good luck!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter
2022-11-05 1:31 PM
Welcome, @AShag.1, to the community!
Theoretically, this might work, but it does not make sense for several reasons, e.g.:
I would recommend looking at the EVALSTDRIVE101 instead, which might suit your needs perfectly.
Does it answer your question?
Regards
/Peter
2022-11-05 2:12 PM
Hi Peter,
Thank you for your reply over the weekend.
Again, thank you for your help.
Best Regards,
Ali
2022-11-06 11:16 PM
You're welcome!
Correct, you would have to adjust the voltage divider R1,2-R4 if you absolutely and against all expectations want to stay with the STEVAL-IPMM10B.
Good luck!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter