cancel
Showing results for 
Search instead for 
Did you mean: 

How to get active power with STPM3x..

LYoun.11
Associate

I am using STPM33.

Reading 70 registers using UART was a success.

Data received ex)

A0 00 E0 04 00 00 00 F8 A0 00 A0 00 E0 04 00 00 00 F8 00 F8 00 F8 00 F8 FF 0F FF 0F FF 0F FF 0F 27 03 27 03 00 00 00 00 7E 77 7E 77 07 40 83 06 00 00 72 10 72 00 08 06 36 02 8C 01 36 02 2A 00 9C 00 F8 FF 9C 00 20 00 B0 00 E4 FF B0 00 11 00 01 80 01 80 00 00 00 00 00 00 00 00 3A FD 4F FD 81 F3 6F 03 00 00 00 00 FF FF 00 00 01 00 00 00 FF FF 00 00 40 FD 59 FD 98 F3 71 03 FF FF 00 00 FF FF 00 00 01 00 FF FF 00 00 00 00 7A FA A8 FA 19 E7 E0 06

The example above is the result of reading it myself.

How can I read the active power from the above data?

0 REPLIES 0