cancel
Showing results for 
Search instead for 
Did you mean: 

How can I activate the internal clock in STSPIN32F0?

TKlei.5
Associate III

How exactly can I program the internal clock in the STSPIN32F0 chip?

2 REPLIES 2
cedric H
ST Employee

Hello

This kind of question is almost impossible to answer without additional information.

I would advise you to download the datasheet, and to start a CubeMX project with a F0 MCU matching the one you have inside your STSPIN.

If you want to build a motor control project with ST SDK, the entry point is the ST Motor Control Workbench provided with the release available here :

https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32cube-expansion-packages/x-cube-mcsdk.html

Regards

Cedric

TKlei.5
Associate III

Sorry.

At the moment I am testing the Steval-Spin3202 board with the STSPIN3202 chip. My problem is that the board is only working if I connect the USB cable.

Is the Steval-Spin3202 board also working without the USB connection?