2022-05-07 12:37 AM
Hello.
I want to drive a BLDC motor with Steval ptool1v1 hardware.
I loaded the example file (6S_Steval_ptool_1v1_HS_WM) into the MCSDK-WB, from which I generated the code (via cubeMX and CubeIDE).
The motor doesn’t work despite all my attempts. Even though potentiometer speed control is included in the user manual as plug'n play(!), I see in the cube IDE it is not implemented. Moreover, I did not find an option in the MCSDK Workbench where this could be selected.
I tried to figure out in the code how to implement it afterwards, but I couldn't figure out the solution.
How could this be solved?
Thanks in advance.
Bela.
Solved! Go to Solution.
2023-01-10 12:06 AM
Hi @Community member
I mean the PWM signals. However you can simply check the phases of the motors at first step. To help you to debug on your side, please consider and check the following anomalous conditions:
Alessio