2021-07-19 10:49 PM
I am using 12V motor, all the phase I measured 12V, its look like it stuck at brake.
what can be the problem?
I am using motor 1028m012b - FAULHABER
Solved! Go to Solution.
2021-09-01 9:16 AM
Hi @IGAL TALOR,
so in summary, the solution to your original question was to replace the damaged motor (Hall effect signal missing), right?
If I understand well, we can consider closed this topic.
Please open a new topic for a new question.
2021-07-20 1:08 AM
Can you show us some picturesof your setup(wiring)?
2021-07-20 1:21 AM
CONNECTIONS:
VS = 12V
J3-16 EN = 5V
J3-6 BRAKE =5V
J3-11 = 5V (its means VREF = 0.9V MEASURED)
J3-4 = 5V (FWD)
all Hall effects connected to motor
all Phased connected to motor
5V and GND supplied to motor
2021-07-20 1:35 AM
2021-07-20 5:03 AM
Hi @IGAL TALOR and welcome to the ST Community.
first I suggest to check the J2 setting: you have to change the default connecting the poles 2-3.
In this way you apply the the 5 V (J3-1) to the VDD net that is used for the Hall effect sensors supply voltage and pull-ups voltage.
Moreover, you may verify also the proper connection of motor:
I would also point out that by applying a VREF voltage of 0.9 V in practice you are disabling the PWM current control (Ipeak = VREF/Rsense = 0.9 V / 0.1 ohm = 9 A!). I suggest to reduce the VREF value according to your target phase peak current.
Let me know is these info are useful to run the motor.
2021-07-20 5:11 AM
HI
J2, I already connected poles 2-3to use 5V.
J5-1 to motor pin 1
J5-2 to motor pin 2
J5-3 to motor pin 3
J7-1 to motor pin 8
J7-2 to motor pin 7
J7-3 to motor pin 6
PWM control no matter at this point, I just want to see that the motor is running.
2021-07-20 6:18 AM
Hi @IGAL TALOR,
please double check the J5 connection.
The silkscreen near the connector indicates the IC OUT number, not the J5 poles number.
If this does not solve the issue, it is necessary to check the device signals with oscilloscope.
2021-07-20 6:29 AM
I connected:
OUT1 J5-3 to motor pin 3
OUT2 J5-2 to motor pin 2
OUT3 J5-1 to motor pin 1
you can see at the motor data sheet that I attached before.
2021-07-20 6:37 AM
I tried to swap between PHASE A and C and the motor is not moving.
2021-07-20 6:40 AM
all the phases A,B and C are with 12V, looks like at brake.