cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I am new to STPM34 eval board and trying to getting start to STPM34 eval software. Getting error "unhandled exception error while doing USB interface"

Madhura C
Associate

On opening the STPM34 eval software and connecting USB to UART to PC.

Under Option>Interface> Communication, I selected Port type as USB and tried to open port.

Error window pop up - 'unhandled exception has occurred' as shown in Fig. 2.

This error remains even if I remove USB to UART from PC.

 Error window: Also, check error details in attached notepad file.

Even after that I continued and selected USB port and open.

'Failed opening IO lib' window pop up as shown in Fig. 3.

Please give me suggestions.

System details:

Model : Lenovo Win7 PC 64 bit

OS : Window 10 Home

Software installed from ST link web site.

Also, installed Virtual COM drivers.

2 REPLIES 2
Madhura C
Associate

I tried on Windows 7. Its working finely.

Is there any window requirement for handling Eval software?

On Window 10, its showing error continuously.

YGebr.2358
Associate

@Madhura C​ I'm using STMP33/34 eval board for my project. and I'm using Windows10 Pro , Works fine.

I think You should select the proper Interface and give separate power to the interface (Isolated 3.3V Supply).