cancel
Showing results for 
Search instead for 
Did you mean: 

Example program needed to setup and use the STM32 pid_regulator?

BTrem.1
Senior II

I'd like to see a simple example program that allows the user to setup the pid_regulator in the STM32 motor code. I'm using the FOC library and want to add an external loop around the speed control to do phase correction. The STM32 code is good at obfuscating all useful information.

0 REPLIES 0