2020-07-07 8:41 PM
we want to develope simple BLDC driver in open loop mode with speed and direction control input.I found your IC L6235 which fits to our requirement .
is there any evaluation kit this IC.
Solved! Go to Solution.
2020-07-08 8:24 AM
Hi @SShin.1 welcome to ST community.
You can use the EVAL6235Q a 3-phase BLDC motor driver board that allows to test the L6235Q functions (L6235 device in QFN package).
The evaluation board can be driven using the STEVAL-PCC009V2 communication board and the PractiSPIN 2 evaluation software (STSW-SPIN003).
I hope I have been helpful.
2020-07-08 8:24 AM
Hi @SShin.1 welcome to ST community.
You can use the EVAL6235Q a 3-phase BLDC motor driver board that allows to test the L6235Q functions (L6235 device in QFN package).
The evaluation board can be driven using the STEVAL-PCC009V2 communication board and the PractiSPIN 2 evaluation software (STSW-SPIN003).
I hope I have been helpful.