2024-03-19 11:58 PM - last edited on 2024-03-20 2:30 AM by Peter BENSCH
Hello There!
I have bought EVAL- SCS001V1 sink device for my application in which I need the output as 12V/2A from the mentioned sink device. I came across below problems and I seek help on it.
1) Problem related to STSW-STUSB002 GUI version 2.0.
The first problem is with the GUI version 2.0 as specified. When I made hardware connections as mentioned in the quick start document and I tried to connect the Nucleo- F072RB with the GUI 2.0, I got an error which says " The Parameter is Incorrect". and I'm unable to connect the hardware with the GUI 2.0.
I have resolved this issue by using the previous version ( STSW-STUSB002 GUI 1.09 ). So my hardware got detected in this version and I was able to program or write the NVM successfully. In the Connection Status of the GUI 1.09 it showed that " OK STUSB4500_L Detected (COM19), at address 0x28 (I2C bus 1)" sharing image below.
2) Problem related to the usage of the source device and selecting desired PDO's.
Currently I'm using the 65W mobile phone charger as the source device. I was not aware of the charging technology it was using. I was not able to switch the PDO profiles at the output. I was getting constant output 5V whereas the required is 12V. So if I'm not wrong the source must be USB PD technology support.
I need help on the available sources which I can use. And how can I select the desired PDO from configured PDO's in NVM to get the desired output 12V/2Amps.
Solved! Go to Solution.
2024-06-05 12:17 AM
Hello,
The .bin file used is "Nucleo_F072RB_STUSB_UART_NVM_config_1.05" which is provided in the package STSW-STUSB002.
I'll send you the waveforms shortly.
2024-06-05 3:29 AM - edited 2024-06-05 5:48 AM
Hello,
Here are the waveforms,
CHANNEL 1: VSNK (Switched to +12V)
CHANNEL 2: VBUS_ENB (Pulse observed)
CHANNEL 3: VBUS (Initially +5V and after negotiation +12V)
CHANNEL 1: VSNK (Not switched to +15V)
CHANNEL 2: VBUS_ENB (Pulse not observed)
CHANNEL 3: VBUS (Negotiation does not happen)
***CC1 AND CC2 SIGNALS
Regards,
2024-06-05 7:14 AM
Hello
on 15V waveform, it seems that there is no messaging on CC lines.
Can you please provide scope snapshot with 500ms total, trigged on CC rising edge (i.e zoom on first part of CC rising edge)
Thanks
Nathalie
2024-06-05 10:35 PM
Hello,
Sending you snapshots for 15V 500ms and 250ms triggered on CC rising edge.
Also below is for 12V 250ms snapshot triggered on cc edge
Regards,
Ashutosh Kedare
2024-06-05 10:53 PM
Hello
As you can see, the source which is supposed to negociate 15V is not responsive.
It seems to be a TypeC 5V source only: there is no messaging from source to initiate any contract. While with 12V source, there is clearly an activity on CC line which reflects the power nego.
Issue is on source side.
Best regards
Nathalie
2024-06-05 11:17 PM - edited 2024-06-05 11:27 PM
Hello,
Currently I'm using this source
I have also replaced the above source with an another source but the same thing happened with it for 15V and 20V profile
Could you please suggest me a source which will work fine and help in resolving this issue. As the issue has been really become critical for us.
Regards,
Ashutosh Kedare
2024-06-05 11:44 PM
Hello
As per the picture, it shall work and stusb4500 will negociate voltage, as per its PDOs, as long as the source sends its source_cap message which is not seen on photo you sent (no activity on CC line).
Best regards
Nathalie
2024-06-06 12:06 AM
Hello,
Yes exactly there is no communication visible on CC line will negotiating 15V but what could be the possible reasons?
Can you please suggest me a source (make and product ID) on which it is tested.
Regards,
Ashutosh Kedare.
2024-06-06 2:22 AM
Hello,
I'm able to get the source_cap message but the profile is not switching to 15V.
Regards,
Ashutosh K
2024-06-06 4:26 AM
seems that something has changed in the setup to get CC communication.
however without being able to see messages in protocol trace, it is nearly impossible to debug.
Best reagrds
Nathalie