2021-10-08 7:34 AM
Hello Sir or Madam,
We have designed an ESC according to STEVAL-ESC002V1 and used ST's 6Step_Library. In our application, There are commutation, noise and maximum speed problem.
What can be the problem or is there another library that we can use for our application?
2021-10-12 1:09 AM
Hi @Yasin Türk and welcome to the ST Community.
Are you using the STSW-ESC002V1 package? It is the reference firmware for the STEVAl-ESC002V1.
You can find more details on the dedicated user manuals: UM2518 for the board and UM2530 for the firmware.
Let me know if these info can help you.
2021-10-18 5:19 AM
Hi @Cristiana SCARAMEL
Yes I am using STSW-ESC002V1 package. I've looked at those user manuals and choosed macros accordinh to UM2530. In UM2736 at chapter 4.5., there is a sense comparators algorithm. We use this algorithm for our application. Is this algorithm applicable for low inductance bldc motors like drone motors?
2021-10-21 4:16 AM
Hi @Yasin Türk,
the firmware you mentioned is designed for drone propellers. It is able to reach higher rpm than the sensorless technique based on ADC.
Did the shared information help you solve your initial problem?
If so please, please click on the "Select as Best" label in the proper answer.
2021-10-24 10:29 PM
We are using this firmware in our project. And there is still noise and maximum speed problem. So, why does not our drone motor reach higher speed? What can be the problem?
2021-10-28 2:33 AM
Hi @Yasin Türk,
concerning to the maximum speed, I suggest to check the supply voltage. A supply voltage even slightly lower than the nominal one of the motor can justify the difference in the maximum speed reached.
About the noise please provide a detailed description of what you mean. Some oscilloscope waveforms could be help (e.g. one motor phase and respective Op Amp signals).
2021-11-01 5:33 AM
Hi Cristiana,
Based on our observations, supply voltage does not change. At the same environmental aspects, Air 40A ESC's noise is 86 dB and our ESC's noise is 92 dB. You can find motor phase and current signals files attached.
2021-11-03 3:37 AM
Hi @Yasin Türk,
please provide the above requested waveforms: one motor phase and respective Op Amp signals in the same screenshoot.
2021-11-30 5:15 AM
2021-11-30 5:19 AM
Hi Cristiana,
I noticed that I didn't add Opbemf1, Opbemf2, Opbemf3 and Opbemf4. You can find them below.
Thanks in advance.