cancel
Showing results for 
Search instead for 
Did you mean: 

dSPIN Evaluation Software control two motors with separate chip selects

jarratt
Associate
Posted on January 28, 2014 at 07:00

Hi,

I have an SPEVAL-PCC009V2 with EVAL-6470H setup controlling one stepper motor very effectively.  I want to control two motors but would prefer to do this using separate chip selects for each L6470 instead of using the daisy chain configuration described in AN3991.  Is is possible to do this?

Possibly related to the above question, is is possible to extend the scripting language in dSPIN to include control of additional IO ports in the STEVAL-PCC009V2?

Thanks,

Bob
1 REPLY 1
Gigi
ST Employee
Posted on March 11, 2014 at 09:33

Ciao Robert

I suggest to post this question in the

https://my.st.com/public/STe2ecommunities/motordriver_ics/Lists/Motor%20Driver%20ICs%20and%20Boards/AllItems.aspx

forum.

Thanks

Ciao

Gigi