2014-02-02 9:10 PM
Hello,
I am seeing a error with the ''SPINFamily Evaluation Software'' when running on Windows XP sp3 on three different platforms.I was able to get the software to operate on a Windows 7 platform, so I am reasonably confident that I am starting up everything correctly and that my hardware is okay.I see a crash as soon as I connect to the board.Details:Windows XP sp3 system [Windows NT 5.1 Build: 2600].Net 4.0 [fresh .NET 4.0 install, fresh sp3 install]SPINFamily Evaluation Software (L6480 selected) [fresh install]According to the message at the bottom of the Spin window the board did connect:Board connected (BR_4MHz) FW Version 0.0This matches what I saw on a windows 7 system that I used to validate that my hardware was okay.Looking a little closer at the error report:EventType : clr20r3 P1 : gui.exe P2 : 1.2.5071.18356 P3 : 528b2b58P4 : mscorlib P5 : 2.0.0.0 P6 : 471ebc5b P7 : 1295 P8 : 14 P9 : system.missingmethodexception Is there a way around this error?Thank you,- Charles. #cspin2014-03-11 1:34 AM
Ciao Charles
I suggest to post this question in the forum. Thanks Ciao Gigi