2024-05-26 11:42 PM
We selected the Triac ST# T1635-600G for refrigerator project, to control the compressor (inductive loads). Tested T1635-600G, the heat is very serious when passing 16A current, even using a heat sink temperature is more than 100°C. Therefore, I want to use T3035H-6G. May I ask how much heat sink is required for this model when it passes 16A? Or do you have app recommendations? Are there any guidelines on heat dissipation? Thank you!
2024-05-26 11:50 PM
Suggest you work with your local rep or support engineer, or submit this as an online support request rather than on the forum.
2024-05-27 12:08 AM - edited 2024-05-27 6:28 AM
just from ds : T16xx :
T30xx :
So at 16A : about 19W -> 16W dissipation with T16 -> T30 ; ( about 20% less , with T30 )
>how much heat sink is required for this model when it passes 16A?
About the same, as with T16 ; but choose T30xx (T16 is at its limit - never good idea !)
>Or do you have app recommendations?
You need more/better heat sink.
>Are there any guidelines on heat dissipation?
Same, as always : the cooler you keep the semiconductor, the longer it will be alive . :)
Here, with 16W loss and desired heat sink temp of about 60° C , at max. 30° ambient you need : (60-30)/16 = 1.8 °/W heat sink. (Or smaller heat sink with forced cooling, using a fan.)
Something like this : (100mm size)
And be aware : triac is not isolated, so need isolated mounting and thermal grease !
2024-05-27 6:20 AM
Please choose the T3035H-6G because is a 150°C max Tj so better in term of dissipation.