cancel
Showing results for 
Search instead for 
Did you mean: 

Can STEVAL_POE002V1 work as 24V source?

WEmme
Associate II

I bought the STEVAL_POE002v1. It works fine at 5 V. Now I want to setup a POE with 24V. Can I achieve this with that STEVAL? I would think to change the transformer and to adjust the Feedback-path and perhaps the Fsw. Can you help me with a calculation example like an Excel sheet or something else?

Many thanks in advamnce!

Best regards

Wolfgang

1 REPLY 1
WEmme
Associate II

Additional question: Do you recommend another STEVAL_*** for this?

Regards

Wolfgang