2019-09-12 5:14 AM
I bought the STEVAL_POE002v1. It works fine at 5 V. Now I want to setup a POE with 24V. Can I achieve this with that STEVAL? I would think to change the transformer and to adjust the Feedback-path and perhaps the Fsw. Can you help me with a calculation example like an Excel sheet or something else?
Many thanks in advamnce!
Best regards
Wolfgang
2019-09-12 5:16 AM
Additional question: Do you recommend another STEVAL_*** for this?
Regards
Wolfgang