cancel
Showing results for 
Search instead for 
Did you mean: 

Can I get any application note on STGPIN3H60 with wave form requirements ,the permitted frequency limits etc.

CVT.1
Associate
 
1 ACCEPTED SOLUTION

Accepted Solutions
uomo motore
Associate III

This info is already available in the datasheet. It has the max frequency limit in the table. There are timing diagrams related to interlocking for the PWM inputs and also for the SmartShutdown function including application information. Do you have any specific query?​

View solution in original post

2 REPLIES 2
uomo motore
Associate III

This info is already available in the datasheet. It has the max frequency limit in the table. There are timing diagrams related to interlocking for the PWM inputs and also for the SmartShutdown function including application information. Do you have any specific query?​

Cristiana SCARAMEL
ST Employee

Hi @CVT.1​,

the @uomo motore's​ answer solved your doubts?

If yes please "Select as Best", otherwise as abovementioned do you have any specific query?

If you feel a post has answered your question, please click "Accept as Solution"