2022-01-17 8:04 PM
Any one have the following configuration.
HW: STM32H753XI-EVAL2
Toolchain: IAR EWARM 8.20.2
Debugger: IAR I-jet
I am getting "Download completed but verification failed." error for the example project UART_HyperTerminal_IT in STM32 MCU Cube Firmware Package Version STM32Cube_FW_H7_V1.9.0
Debugger always throws error: Download completed but verification failed.
Note: With IAR v8.22.2, I was able to download few time. It was failing randomly. After downgrading to 8.20.2 it is failing always.
I did downgrade IAR version to match with one the demo project(STM32Cube_FW_H7_V1.9.0) was developed.
Solved! Go to Solution.
2022-01-19 2:33 PM
Tried the STM32 Cube Demo projects. The results are same. Verification Failed. Confirmed by using Cube32 programmer and reading flash memory.
Recovered through the following.
After the upgrade, its OK now.
2022-01-19 2:33 PM
Tried the STM32 Cube Demo projects. The results are same. Verification Failed. Confirmed by using Cube32 programmer and reading flash memory.
Recovered through the following.
After the upgrade, its OK now.
2022-01-19 2:40 PM
So working now?
Watch for board level conflicts, correct Flash banking options/settings. Check cross connectivity of SWDIO, SWCLK, SWO(TDO/PB3), NRST. For Trace check jumpers related to high order address bits on FSMC.
Current DLLs for ST-LINK, both IAR and KEIL
Note patches for various tools are in the repository
STM32Cube_FW_H7_V1.8.0\Utilities\PC_Software\IDEs_Patches\EWARM\EWARMv8_STM32H72x-73x_Support_V0.2.zip
2022-01-19 3:28 PM
Yes. Upgraded to IAR v9.10.2. Working fine with both STLINK and I-jet.
Thanks for patch details. I haven't applied the patch yet. Will install the same.