Skip to main content
Associate
May 15, 2025
Question

STM32G071CBT7 overcurrent

  • May 15, 2025
  • 6 replies
  • 558 views

Hello, I am an engineer developing a board using STM32G071.

 

Currently, I am using all pins of the MCU, SPI, I2C, and GPIO, but one of the products is overheating and overcurrent is occurring.

The existing consumption is 30mA, but the problematic product consumes 110mA. I would like to inquire about which pin of the MCU can cause overcurrent to flow.

Or, if you tell me a case where overcurrent can occur in the STM32G071, I will check it out.

This topic has been closed for replies.

6 replies

LCE
Principal II
May 16, 2025

Have you checked the package pins for any shorts?

Same with any external loads? E.g. pull-ups / downs, power, filter caps, ...

SJKwonAuthor
Associate
May 16, 2025

This issue does not occur on all boards that utilize MCU.

 

This is an issue that occurred during a restart while in use.

Andrew Neil
Super User
May 16, 2025

If it only happens on one board, that suggests there is a fault on that board.

So carefully inspect that board for:

  • Shorts or solder bridges
  • Incorrect components fitted
  • Misaligned or incorrectly oriented components (including the MCU itself)
  • etc, etc, ...

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
SJKwonAuthor
Associate
May 21, 2025

The MCU board and power board are connected with a board-to-board connector, and an overcurrent phenomenon occurred in a product where the connector connection was unstable.

I am currently using both MCUs (LQFP48), but which two pins could cause an overcurrent phenomenon if they were shorted?

Andrew Neil
Super User
May 21, 2025

Your description is far too vague to make any specific comments.

You need to show full schematics.

Also some good, clear photos of the system.

Remember that we know nothing about your system other than what you provide in your posts; we can't see it, we can't investigate it for you.

Tell us what tests & measurements you've done to find where this excess current is going.

How to write your question to maximize your chances to find a solution.

 


@SJKwon wrote:

The MCU board and power board are connected with a board-to-board connector, and an overcurrent phenomenon occurred in a product where the connector connection was unstable.


Are you plugging/unplugging while the power is on?

When you do that, you need to ensure that things connect/disconnect in the correct order - so you don't get power applied to IO pins before the supply is connected, etc ...

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
LCE
Principal II
May 21, 2025

Any 2 pins that don't have the same voltage level...

Ever heard of Ohm's law? V = R * I 

;)

But because of the difference being that high, it looks more like some power and / or GND pins are involved.

Maybe some power supply shorted to an GPIO set to output with low level.