cancel
Showing results for 
Search instead for 
Did you mean: 

No STM32 target found

Seba_Grae
Associate II

Hi friends, I'm having a problem with my MKS Odrive Mini V1.0 board.
I replaced the MCU because the old one had shorted out.
The problem is this: the board is no longer recognized by USB.
I'm trying to use an STLink, but I also don't have access to load the .hex file it comes with. I would need your help to try to flash the new MCU somehow.
I was using both STM32CubeProgrammer and STM32Utility, but neither of them worked.

5 REPLIES 5
mƎALLEm
ST Employee

Hello @Seba_Grae and welcome to the ST community,


@Seba_Grae wrote:

 I'm having a problem with my MKS Odrive Mini V1.0 board.


This is not a ST product. So you need to provide more details about this board. Links, schematics etc ..

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

I'm sending the schematic so you can see if you can help me.

Andrew Neil
Super User

Welcome to the forum.

For best results, please see: How to write your question to maximize your chances to find a solution

In particular, as @mƎALLEm said, you need to give details of this 3rd-party board.

Also what version of CubeProgrammer did you use?

Please post the full log from CubeProgrammer when trying to connect.

 

Are you using a genuine ST-Link?

See: How to recognize a genuine ST-LINK/V2 versus a cloned one.

In particular, anything looking like this is a fake/clone.

 

Note that the ST-Link Utility has been obsolete for years.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

STMCubeProgrammer 2.20.0

ST-Link V2 Clone
STM32F405 RGT6 is the MCU that has the board

I send the connection attempt file.

I don't know what additional information might be useful to you.